In the News | Daikin Applied

 

In the News


Archive by month: 2020-2Return
February 25, 2020 | Chiller & Cooling Best Practices | Two water-cooled chillers were on display at the Daikin booth.
February 23, 2020 | Cooling Post | Daikin Applied is set to introduce its first chillers based on the low GWP HFO refrigerant R1233zd.
February 5, 2020 | Contractor Magazine | A lot of foot traffic over by the Daikin booth at AHR.
February 5, 2020 | Buildings | At the AHR Expo 2020, experts in sessions and on the show floor discuss what they’re seeing in the field today from the impact of the climate crisis, including major moves toward decarbonization and a stronger focus on indoor air quality.
February 5, 2020 | ACHR the News | New products will offer increased capacity and energy efficiency than R-410A
February 5, 2020 | Contracting Business | Combination brings efficiency that exceeds the new minimum requirements for 2023.
February 4, 2020 | Facilities Net | Rebel Applied is small and light, featuring a high-efficiency motor, compressor and other components.